Press releases 2024

The boring bar holder GARANT Master Eco VDI E2 is extremely easy to handle thanks to the new clamping concept and operating instructions lasered onto it.

Clamping long boring bars with repetition accuracy using just a single screw

18 Nov 2024

New GARANT Master Eco VDI boring bar holder E2 now available with adjustable clamping range, new clamping concept and three-stage cooling system Efficient Cooling (ECO).is now available.

The GARANT GMT2 vibratory finishing machine deburrs and polishes individual parts and small batches to a high quality in a dry process.

Compact, easy, efficient: the GARANT GMT2 vibratory finishing machine handles individual parts and small batches in next to no time

10 Sept 2024

GMT2 delivers top quality deburring and polishing results on turned, milled and 3D printed metal and plastic components using dry machining.

The new GARANT Master Steel solid carbide drill is designed for universal use with a range of different steel and cast materials.

With GARANT Master Steel, the Hoffmann Group opens up a new performance class for double-edged solid carbide drills

10 Sept 2024

The extremely stable solid carbide drill bit with S-cutting edge and special tip achieves up to 30% higher removal rates and twice the tool life.

The GARANT GreenPlus solid carbide end mill is made in a low-CO2 production facility.

AMB 2024: World première for the first GARANT GreenPlus solid carbide end mill made of 99% recycled carbide substrate

10 Sept 2024

The GreenPlus milling cutter brings more sustainability to machining.

2024/2025 Hoffmann Group catalogue available as an online flip catalogue; all items also available in the eShop

22 Jul 2024

The Hoffmann Group is committed to sustainability and publishes a print catalogue every two years, the most recent version last year.

The new "Tool Assembler" functionality makes it possible to deploy all employees with relevant programming skills more efficiently.

Configure entire tools without a CAM system and manage them in the centralised tooling database

18 Jun 2024

The new “Tool Assembler” functionality allows users to assemble entire tools in the Connected Manufacturing digital production solution and search for components in 49 manufacturer catalogues.

Saves space and is easy to operate: automated clamping device handling with the GARANT Turntable

18 Jun 2024

New loading system with start/stop pin mechanism is smoothly simple and inexpensive to connect to any CNC milling machine.

As the event took place during the European Football Championship, the Bavarian Minister President Dr. Markus Söder signed a football, which was auctioned off for the benefit of the Hoffmann Group Foundation.

Europe’s most cutting-edge tool logistics facility officially opens in Nuremberg

18 Jun 2024

Hoffmann SE has invested more than 200 million euros in LogisticCity.

With its seven extra-sharp cutting edges, the GARANT Master Alu solid carbide finishing cutter can even machine 90-degree corners and edges with a high level of precision.

Fine finishing of aluminium with low infeed

8 May 2024

GARANT Master Alu solid carbide HPC finishing cutter with seven cutting edges produces top-quality surfaces with low infeed during profile milling.

The Hoffmann Group’s in-house exhibition “World of Tools 2024” will take place from 18th to 20th June 2024 in Nuremberg.

World of Tools 2024: Dedicated to efficient production, digitalisation and automation

16 Apr 2024

Hoffmann Group organises in-house exhibition with over 115 exhibitors and celebrates the world premiere of a new automated GARANT loading system.

From left to right: Holger Quade, Senior Director Compliance, Risk & Sustainability at Hoffmann SE; Simon Barber, Senior Manager ESG at Hoffmann SE

From bronze to silver: Hoffmann SE moves up the EcoVadis sustainability ranking

21 Mar 2024

Hoffmann SE has improved its EcoVadis sustainability rating from bronze to silver.

Sign in

Login

Your contact person

Set commission

Your customer card

Please present the QR code at the checkout.
Retrieved on 
To shopping cart