A+A 2025: Individual and sustainable protection from head to toe
1 Jul 2025
The Hoffmann Group will be represented at the A+A in Düsseldorf from 4 - 7 November 2025, in Hall 12, Stand E36. As well as presenting its full range of personal protective equipment (PPE), the focus at the trade fair will also be on intelligent industrial vending systems and sustainability. In addition, attractive services and consulting offers on topics such as risk assessment, product selection and customisation, documentation and training will be presented. Live demonstrations and try-on tests directly on site turn a visit to the trade fair stand into an experience.
The Hoffmann Group’s product range currently includes around 6500 PPE products from 60 leading manufacturers as well as products from its own GARANT and HOLEX brands. Accompanying its product range, the Hoffmann Group provides advice to companies throughout Europe on selecting PPE articles and consolidating them in a standard catalogue, provides assistance in consolidating the supplier file, and thereby creates the basis for further automation of the procurement process. GARANT Tool24 and HOLEX 24seven industrial vending systems play a key role in this process. In this context, as a trade show first, the Hoffmann Group will be presenting the weighing cell system.
It enables items to be removed intuitively, with user logon using RFID technology. Thanks to high-quality weighing cells, the system automatically detects which items have been withdrawn. The weighing cell system is available at an attractive entry-level price of €11,900. Further benefits are:
- Easy to fill: removable boxes and automatic recognition of the stored items provide complete system access.
- A high degree of flexibility: with three container sizes and a maximum of 70 boxes, the system can be individually configured.
- Management of third-party items is possible.
Another highlight of the trade fair are individual and attractive PPE solutions which can be tested directly at the stand. The Hoffmann Group is able to provide personalised workwear in corporate designs by offering various textile customisation options, such as embroidery, to apply a high-quality company logo, claim or name to the clothing.
In the field of protective gloves, experts provide support in finding the right product - including the creation of a customised glove plan for employees based on a risk assessment. The plan also serves as documentation and defines which gloves are suitable and should be used at which workstations and for which activities.
In addition, there are individual foot analyses using 3D scanning and other bespoke protective equipment solutions, including professional advice that considers all the different manufacturers. The benefits: optimum safety and high wearer acceptance thanks to a high level of comfort.
In keeping with the A+A 2025’s trend topic of ‘sustainability’, selected, environmentally friendly and durable products will be exhibited again this year. The GARANT products in the GreenPlus series combine sustainability and efficiency to a unique degree: from cleaning to personal protective equipment such as breathable clothing, ergonomic work shoes or sustainable protective gloves.
Other bespoke solutions for future-proof workplace design as well as short delivery times, a delivery capability of over 99 percent and delivery accuracy of over 99.9 percent round off the Hoffmann Group’s offer. In Germany and bordering regions, the goods usually arrive at the customer within 24 hours of receipt of order. The standard delivery time across Europe is usually 48 hours.